7/20/2011 10:21 AM | |
Posts: 157 Rating: (10) |
Dear Mohammedwaly, See this link: Regards,
|
Last edited by: BilalD at: 7/20/2011 10:21 AM |
|
7/21/2011 1:30 PM | |
Joined: 3/15/2010 Last visit: 6/18/2024 Posts: 137 Rating: (9) |
The SQL archives in WinCC are encripted, so I believe it is not possible to access the tables directly. One solution is the one suggested by BilalD, that is using the export to CSV function in the Trend Control. Another solution is to access the archives using OLEDB. Please try the excel file in attachment to see if you can do this. AttachmentOLE-DB Tag and Alarm Export.zip (1059 Downloads) |
7/22/2011 11:55 AM | |
Joined: 9/8/2005 Last visit: 9/11/2024 Posts: 177 Rating: (15) |
Hi, an easy way to export WinCC archive data and other values is to use the WinCC Add-on PM-OPEN EXPORT. The programm allows you to export data into a ASCII based file (e.g. csv, txt, html,XML, ..). So it is possible to write alarms, tag logging values, user archive values, online tags to this file. More information about PM-OPEN EXPORT: www.siemens.com\pm-open-export Michel |
5/24/2017 3:26 AM | |
Posts: 7 Rating: (0) |
Hi mnguira, The file that you gave us here only suports windows 32bit. Do you know any file that support windows 7 64bit. Many thanks |
5/24/2017 11:45 AM | |
Joined: 3/15/2010 Last visit: 6/18/2024 Posts: 137 Rating: (9) |
Sorry I don't have any other version |
Follow us on