9/18/2012 9:38 AM | |
Posts: 7 Rating: (0) |
Hello guys! I have an old OP 15 C1 panel (6AV3515-1MA20-1AA0), firmware 2.30 and I want to put a new configuration on it. I delete the old configuration on it by pressing ESC - RIGHT - DOWN keys when powered up. I made myself 2 cables - see the attachment for schemes, because I am not sure witch one is good. I have windows 7 x64 and the protool doesen't work on that, so I made a Virtual Machine with windows xp, installed protool and everything was good. Now the problem appeares when I try to download the configuration. With the both cables its the same error in protool: E4017: Protocol error with serial connection for lines FFFF021BH. If you need more info to help me let me know. Thanks guys! AttachmentCables.zip (599 Downloads) |
9/19/2012 5:02 PM | |
Posts: 3037 Rating: (192)
|
Hello iosubvictor, You can use this cable to download your project to an OP 15. See the following link. What is the serial cable assignment for transferring the configuration to an RMOS operator panel? Tweety |
9/19/2012 5:14 PM | |
Posts: 7 Rating: (0) |
Yes, thats the cable I made it. See attachement 1. But still... that error. Any other ideas? Come on guys! Thank you! |
5/26/2017 8:23 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by AFCI is split to a separate thread with the subject Load the configuration to OP15. Best regards |
Follow us on