5/24/2017 4:55 PM | |
Posts: 1 Rating: (0) |
Hi Does someone knows where to find a manual about how to program IOT 2020 in Arduino, adding to this, I have got a problem, it seems is not possible to use the instrucction .toFloat() in IOT siemens, is it possible to convert String received from serial to float??? Thanks Miguel ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/26/2017 8:55:49 AMNew subject after splitting |
|
5/26/2017 12:14 PM | |
Posts: 37 Rating: (3) |
Hi,
The libraries shipped together with the download of the Galileo device package are too old for your source code. If you want, you can download the current development release from here. You should keep the original files directly placed in "packages/Intel/hardware/i586/1.6.7+1.0" and only update the files in the following folders:
Michael |
5/29/2017 8:32 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, You can find a tutorial how to use Arduino IDE with IOT2000 here: https://support.industry.siemens.com/tf/ww/en/posts/running-arduino-sketch-on-iot20x0/157577/?page=0&pageSize=10. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on