2/25/2011 9:03 AM | |
Posts: 376 Rating: (57) |
hello aiden25, between a Field PG, Power PG or PG7xx and the programmable controllers fromSIMATIC S5AG 90U to AG 155U you can use the cable with the order number 6ES5734-2BD20. More information about the cable finds you here: http://support.automation.siemens.com/WW/view/en/217863 If your customer uses a PC with serial RS232 interface he can take the PC converter cable with the order number 6ES5734-1BD20. The interface assignment of the PC converter cable finds you here: http://support.automation.siemens.com/WW/view/en/13063839 Here a further recommendation. Köster-Box (PC-S5-Interface) Interface for programming Siemens S5-PLCs with the PC. The Kösterbox converts the RS232 signals of the PC into TTY signals (20mA) of the automation system. • The box is full duplex, send- and recieve channel, • the box is active for programming SIMATIC S5 AG90 - AG115U, • for S5-135/155U and CP or acting passively with other cable, • the box has its own power supply with galvanic separation Her the link: http://www.koester-systemtechnik.de/Koester_Box_E.html Best regards Gucci |
2/25/2011 5:37 PM | |
Posts: 74 Rating: (2) |
Hello aiden25, You can try also http://www.helmholz.de/prod,48_49.html Good Luck Vitas |
2/21/2017 3:21 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by norimane is split to a separate thread with the subject Step 5 Error, AG-zeitueberlauf. Best regards |
7/3/2017 6:41 PM | |
Joined: 4/12/2016 Last visit: 4/25/2023 Posts: 2 Rating: (0) |
I would just add that I am using Westermo MA-21 TTY modem as an active converter. It has the same spec as the Koster box described in previous post. Maybe not the cheapest and comfortable solution, but probably the most stable and quality converter. I had few of those at my company doing nothing. They were used for printers connected to S5. Just had to make cable for 95,135,155 and one for 150U latest model in production at the time of posting http://westermo.com/products/converters/current-loop-converters/md-21-ac |
Follow us on