7/11/2017 5:50 AM | |
Posts: 41 Rating: (0) |
Hello experts. I'm running old 840D from year 2000 simodrive 611 with SW 4.4 I have made a 5 axis post processor for NX that work with 4 axis programing with Arot X Y Z milling and C and B axis position is good. My problem is when I want to make a full 5 axis program where it out put the NC code by using MCS compared to the work part the position of my tool dont match the NC code position it looks like its offset by 40mm smaller. I have programed it with a 16mm end mill. can anyone tell me if I'm missing a G code in my nc code? attached is 2 nc programs Full 5 axis program (this is the problem nc file) 5 axis program working. I cant figure out why the tool position is not where the actual WCS coordinates are, please write if you need me to give anyone screens or additional information. regards Flemming Attachmentprograms.zip (82 Downloads) |
Follow us on