1/26/2013 2:28 PM | |
Joined: 8/31/2010 Last visit: 9/20/2024 Posts: 1521 Rating: (227) |
Hello ARN2011, AttachmentE:\ModbusTCPIP.pdf (3694 Downloads) |
Like it? Rate it! |
|
1/28/2013 7:20 AM | |
Joined: 7/16/2011 Last visit: 8/16/2024 Posts: 24 Rating: (0) |
Hello UMENCHO |
2/2/2013 4:45 PM | |
Joined: 7/16/2011 Last visit: 8/16/2024 Posts: 24 Rating: (0) |
Dear Yolov, Thank you for your post. So it shows it will be possible to connect to non-modicon PLC's. Best regards |
7/3/2017 11:46 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by H.M.Suleman is split to a separate thread with the subject How many Modbuses can create in tag management?. Best regards |
7/17/2017 11:20 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
Hi, As you could see from others people answers, there is no guarantee that Modbus TCP driver from the WinCC will work with non-Modicon (Schneider) PLC's. Some devices that fit the protocol, will work. Some others - will not. However, some OPC server with Modbus TCP connection solves the problem. OPC's of this kind are usually not for free, but I have found several very, very cheap solution, easy to engineering, and reliable. I am sharing one with you, that saved my life :) http://www.lectussoft.com/
Best regard, |
This contribution was helpful to1 thankful Users |
Follow us on