7/20/2017 4:24 PM | |
Joined: 5/16/2016 Last visit: 9/24/2023 Posts: 6 Rating: (0) |
Dear As additional information, now when testing with SCOUT version V4.1.5.15 brings me the axis positioning configuration, but not the configuration of inputs and outputs, nor the statements with the associated logic in ST or LAD languages. The warnings are as follows: Information: C230: Information 5056 Upload for device C230. Warning: C230: Warning 5067 The object identifier uploaded from object C230 cannot be accepted. Consistency through download. Warning: C230: Warning 5085 No additional data found for the device. Recovery not possible. Information: C230: Information 2001 Checking the technology packages... Information: C230: Information 5080 Loading 'execution system' configuration to PG... Warning: C230: Warning 5079 No additional data found for the 'execution system' configuration. Complete recovery of the 'execution system' configuration not possible. Information: C230: Information 5082 Upload: The data on the card has been created with a version < 4.1. It is not possible to align the 'execution system' configuration with this data. Information: C230: Information 2120 Loading additional data of the IO variables to the PG... Warning: C230: Warning 2130 No additional data found for the I/O variables. Recovery not possible. Information: C230: Information 2059 Checking the default values of the device variables... Information: C230: Information 2102 Checking the TO configuration... Information: C230: FeederAxis: TO C230: FeederAxis is consistent - upload skipped. Information: C230: Information 2102 Checking the TO configuration... Warning: C230: Warning 2131 No additional data found for the global device variables. Recovery not possible. I would appreciate any additional comments Attachment19-07-2017_Output window.txt (254 Downloads) |
7/20/2017 9:08 PM | |
Joined: 5/16/2016 Last visit: 9/24/2023 Posts: 6 Rating: (0) |
Right. Thank you very much for your help. |
Follow us on