1/12/2017 1:39 PM | |
Posts: 35 Rating: (0) |
Hello Forum, I am having 20 devices of 3rd party, which I need to communicate with them through Modbus RTU - RS-484 - 2 Wire mode. I was pretty clear in configuring them. Config: S7-400H with ET200SP modules having 1 Modbus Comm Module. I had only 1 clarification, all the devices I connect are of same baud rate & same communication settings. So, I will use 1 - Modbus Comn Load & 20 Modbus Master blocks. For every, Modbus master block, there will be an DB generated & that DB need to be linked Modbus Comm Load (MB_DB) parameter. So, for other 19 DB, where i need to connect to MB_DB OR I have call 1 Modbus Cmn Load & 1 Modbus master as an set of 20. please help...! ------------------------------------------------------------------------------------------ |
Last edited by: LKMNVRS at: 1/12/2017 1:40:25 PMLast edited by: Min_Moderator at: 1/12/2017 2:21:43 PMNew subject after splitting |
|
6/27/2017 9:49 AM | |
Posts: 3 Rating: (4) |
Did you resolve this? I've got some experience with multiple 3rd party devices connected via Modbus RTU to ET200SP CM. |
7/26/2017 7:35 AM | |
Joined: 6/19/2017 Last visit: 4/24/2024 Posts: 7952 Rating: (162) |
New question published by LHotan is split to a separate thread with the subject S71500+ET200Sp modul with CM ptp module on ET200Sp - Has someone an example about this configuration?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on