9/27/2010 12:50 PM | |
Posts: 101 Rating: (11) |
Hi, The pining you can find in the S7-200 system manual in the link above..
The PPI cable is a simple data-driven RS232-RS485 converter, powered by the PLC. The pin configuration for the RS232 side is:
|
This contribution was helpful to2 thankful Users |
9/27/2010 1:05 PM | |
Posts: 101 Rating: (11) |
The attached might be helpful. Thanks, Attachments7200cableEnglish[1].pdf (3398 Downloads) |
This contribution was helpful to2 thankful Users |
9/27/2010 1:10 PM | |
Posts: 101 Rating: (11) |
Setting the PG/PC interface config for the baud rate: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=11870489&caller=view Thanks, |
This contribution was helpful to1 thankful Users |
9/28/2010 6:32 AM | |
Posts: 18 Rating: (0) |
Dear radekk, I have also same problem as well as like you at this time i have notdown pin configuration So, i will send you this configuration in attachment(pdf file) pls find it. AttachmentUSB_PPI ADAPTER 9-PIN D-TYPE CONNECTOR DETAIL.pdf (2288 Downloads) |
This contribution was helpful to5 thankful Users |
7/26/2017 10:49 PM | |
Posts: 2 Rating: (0) |
And for clarification the adapter that I am working with has the following part number. 6ES7 901 3CB30 0XA0, RS232 / PPI Multi Master |
Follow us on