7/23/2017 8:08 AM | |
Posts: 2 Rating: (0) |
I know s7 400 is advanced plc compare to s7 300 plc. But how advanced ? |
7/23/2017 1:53 PM | |
Joined: 9/27/2006 Last visit: 5/12/2024 Posts: 12257 Rating: (2666) |
Hello umang; Ten years ago, the difference between the 2 families would have been evident: the S7-400 was considered a high-end controller, with higher processing speeds.larger number of I/Os.more communication interfaces and specialized modules than the mid-level S7-300. Today, these differences have been largely reduced. The newer S7-300 CPUs have comparable processing power and can use networks (Profibus and Profinet) to extend the number of controlled I/Os. The only remaining factors distinguishing the two families are Hot Redundancy (S7-400H Systens) and PCS 7 (which is based on the S7-400 processors); thés features are not as easily available for the S7-300. There are many threads on the subject on the forum, search for them for further details. Here is one: Difference between S7-400 and S7-300 https://support.industry.siemens.com/tf/ca/en/posts/32342 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/23/2017 1:54:43 PM |
|
This contribution was helpful to2 thankful Users |
7/23/2017 4:49 PM | |
Posts: 2 Rating: (0) |
thanks Daniel chartier |
8/14/2017 10:17 PM | |
Joined: 6/27/2016 Last visit: 4/30/2024 Posts: 11 Rating: (1) |
additional to these, there are extra accumulators "accu3 & accu4"
|
Follow us on