8/18/2017 12:41 AM | |
Posts: 17 Rating: (0) |
Hi I have to communicate the Atlas Copco G250 to Siemens S7400 PLC. I already installed the GSD file and I have the program . The problem is I didn't get data from the compressor. It gives an error in the receive side : the highest bit of Byte_1 , the Node Address, is set to 1 and the error code in the Data record is 1 : Node Address Not found. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/18/2017 1:21:04 PMNew subject after splitting |
|
Follow us on