8/17/2017 8:23 AM | |
Posts: 15 Rating: (0) |
Hello to all, it looks like we always find a way to broke our Ethernet connection with the PG/PC interface. Here is my case: System: Microbox PC420 with WindowsXP Originally installed software: Step 7 5.4, WinCCFlexible2005, Simatic NET, STARTER, DRIVE ES. The Microbox is used only to run WinccFlexible2005 as an HMI and to do all the tasks usually needed by a process, change parameters, trend data etc...Due to the obsolescence of WinCCFlexible 2005 and as apparently some password protected screens were inaccessible we upgraded the WinCC to the 2008 version. To do this was necessary to upgrade WindowsXP SP2 to SP3 as WinCCFLexible 2008 is only compatible with WindowsXp SP3. After the Windows upgrade and after the WinCCFlexible upgrade we were not able to get online. We always get this message when attempting to change the communication configuration path.The properties of this CP cannot be selected here. You have two possibilities to change the properties of this CP. We uninstall Step 7 the reinstall it bu it still the same. We also did the UMENCHO procedure and didn't work. The service is not running and it cannot be started from the services. Any help on this matter will be must welcome. Regards, IA ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/17/2017 1:54:34 PMNew subject after splitting |
|
8/23/2017 3:54 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12856 Rating: (1639) |
Hello I A do you use a Simatic Net configuration?? Or do you use without? In both cases here ist the manual: https://support.industry.siemens.com/cs/ww/en/view/42918861 Hope it helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on