8/23/2017 11:42 AM | |
Posts: 13 Rating: (1) |
Dear all, Many thanks for your support. We successfully expanded the context menu and we are able to call our own script directly from the P&ID. Now we have the following challenge. The script needs some information that changes for each project. Therefore we have created a tab for "customer-specific project properties" and defined there two attributes. Now, the script is saved on S01 @20/A80/Z10/. We are trying to call the project specific properties from the script in this way: ' Set Proj = Project The problem is that when we call the script from the Planning project by clicking on the context menu of the engineering object The script searches this two attributes on the S01 project. How can I do in order to make COMOS take the values from the planning project where we are calling the function and not from the SO1? Many thanks in Advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/24/2017 12:31:53 PMNew subject after splitting |
|
8/23/2017 9:54 PM | |
Joined: 1/2/2017 Last visit: 4/14/2024 Posts: 209 Rating: (117) |
Hi, Use Context.ComosObject.Project Jiri |
8/24/2017 11:20 AM | |
Posts: 13 Rating: (1) |
Tank you! there was a problem with CallScriptLib. Now its working fine. |
Follow us on