8/29/2017 2:10 PM | |
Joined: 3/31/2015 Last visit: 1/26/2024 Posts: 175 Rating: (16) |
Just to confirm - are you experiencing F2 during braking? |
8/30/2017 10:02 AM | |
Joined: 8/29/2017 Last visit: 11/9/2023 Posts: 10 Rating: (1) |
I have a litle experience with micromaster and this faults, what kind of control are you using?, P1300?, and what applicattionare made? Normally this fault is corrected with an external braking resistor. Are you tried to increase the P0210 to 400V? If you have time, there are on the support a script to read values like the trace function. Only for confirm the peak values of the DC-Level. Attachment55652880_faq_starter_script_trace_for_mm4_and_g120_en.pdf (207 Downloads) |
Follow us on