4/26/2013 12:01 PM | |
Posts: 2964 Rating: (479)
|
Hello, F-09 tells us Fault in the motor encoder system... Possible cause: Motor encoder not connected or defective Motor encoder cable defective Measuring circuit 1 (speed actual value sensing) defective, not correctly inserted or incorrectly equipped (P–150).The fault message can be suppressed via P–090 bit 1 from FW 2.00 onwards.Removing fault: Check the encoder cable/shielding, or Replace the motor encoder, or Replace the control board |
9/12/2017 9:14 AM | |
Joined: 6/19/2017 Last visit: 5/13/2024 Posts: 8025 Rating: (163) |
New question published by bsafak is split to a separate thread with the subject Can ı use 6sn1122 instead of 6sn1121?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on