9/13/2017 7:43 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684)
|
Hello tomi; Th Siject system is quite old, the documentation I have located points to Simatic Manager v5.0 as programming software, along with a PC-Adapter (RS 232 to MPI: 6ES7972-0CA23-0XA0). In my experience a USB variant of any adapter can easily cause connection issues if the system does not support the drivers. Siject 15/16, New Start-Up, SW Version 1, Technical Manualhttps://cache.industry.siemens.com/dl/files/187/13051187/att_66544/v1/SIJECT_Customer_Info_1.1E.pdf Before we move on to changing your hardware or software, let's check what you have on hand: How have you set up the USB PC adapter? MPI protocol, 187,5 kB, "only Master on the bus" checkbox? What have you put as access point? Have you tried the PG/PC diagnostics folder? Do the Power (USB 5V) and Activity LEDs light up when you connect to the CPU; do they flash? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/13/2017 8:09:47 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on