9/28/2017 11:46 AM | |
Joined: 1/27/2012 Last visit: 6/20/2024 Posts: 84 Rating: (1) |
Hello all, I have a PC station which will work as ES/OS functionality. This station will have Step 7 Pro 2017, Wincc Advnced V14 SP1 and WinCC Advnced Runtime V14 SP1 software. How can i use the load and transfer of project to the same PC station. I want to restrict the edit of the HMI project. So I am not considering to start of runtime from the configuring software. How can I restrict the Project configuration software and only start PC runtime for the operator. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/29/2017 8:39:52 AMNew subject after splitting |
|
Follow us on