10/7/2017 3:37 PM | |
Joined: 6/9/2017 Last visit: 10/29/2020 Posts: 5 Rating: (0) |
Hi, we have a phisical Machine Win10 Pro 64 bit with TIA Portal V14 SP1 Upd3 (Step 7 e WinCC Professional) used until now only for project PLC, WinCC Advanced and Panel without problem. Now we should develop new WinCC Professional project The problem is: - Opening a project with a WINCC Pro station (new project or existing project make in other PC) an error appear during saving or compiling (see attached) - The other PLC and WinCC Pro function seems to be ok (page, tags, archive, etc. The problem seems to be related to SQL Server. Any idea? Thanks AttachmentErrori WinCC Pro V14 SP1 UPD3.xlsx (42 Downloads) |
Follow us on