2/21/2013 9:44 PM | |
Posts: 2 Rating: (0) |
can't i only transfer the system block by only copying it from another unpassworded plc |
This contribution was helpful to1 thankful Users |
2/10/2014 9:14 AM | |
Posts: 340 Rating: (6) |
new question is splittet toHow can i create a backup file from cpu 224 that has no eeprom |
10/8/2017 3:42 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello, If you can connect to PLC but con't access application due to un-known password, you can use master password "CLEARPLC". But be careful, because it will erase the application on the CPU and you will need to program it once again from scratch. Another way, if you cannot connect to the CPU due to un-known address / baud rate, then you can use WIPEOUT tool: Resetting the S7-200 to the factory default settings (WIPEOUT) Hope this helps. |
Ayman Elotaify |
|
Follow us on