10/5/2017 3:39 PM | |
Posts: 62 Rating: (0) |
Hello, we have milling machine with 4 axis and spindle X , Y and Z are linear axis and A is rotary axis. I would like to cut a circle on the pipe in order to use the linear axis X and the rotating axis A. But I don't know which function I must use. I try with G07.1 and machine have problem with syntax error. So i want to rotate the pipe and moving tool in the X coordinate left and right to cut circle in the pipe. I attachment a sample of NC program. With sample program is a problem in this that A axis wait for each degre. It's go like this : 90-->stop-->91-->stop-->92-->..... I dont know how to solve this problem. Can you pleas help me. Thank you Attachmentnew 1.txt (28 Downloads) |
Last edited by: jkrive at: 10/5/2017 3:40:19 PMLast edited by: jkrive at: 10/5/2017 3:41:31 PMLast edited by: jkrive at: 10/5/2017 3:42:02 PMLast edited by: jkrive at: 10/5/2017 3:44:20 PMLast edited by: Jen_Moderator at: 10/6/2017 8:37:35 AMEdited post for better reading. |
|
10/8/2017 2:48 PM | |
Joined: 1/19/2008 Last visit: 4/19/2024 Posts: 980 Rating: (63) |
Hi, Have you got G64 active ? Pee |
Follow us on