9/24/2013 1:29 PM | |
Posts: 10 Rating: (0) |
Dear Yolov, my comment about #3. I new in WINCC, so may be there ere many wrongs from me, – in attached screenshots I try to explain what I mean. Help please.
One more question – is there ways to create templates (like WINCC flex, or Citect) – it must be background page with common information (Current user, Date/Time ect.) and navigations.? …How every page can include this template. In forums see topic about layers – but can not understand, how layers can be tamplaytes. Thank You so much Attachmentfaceplate.zip (854 Downloads) |
9/24/2013 4:59 PM | |
Joined: 2/22/2006 Last visit: 3/29/2024 Posts: 290 Rating: (37) |
Hi, Finally I understand what you mean! You are talking abou faceplate instances! Faceplate instances are good for intelligent symbols! They are simillar to customized object (with their cos and pros of course). Attached is an example of one of my faceplate instances. I hope it will help you. The faceplate instance is done by WinCC v7.0 SP3. For the rest of you questions - regarding faceplate for displaying information for the object. It has to be done with the means of WinCC. Please have a look on WinCC demo project. There are good example of faceplates. Here is the link: https://support.automation.siemens.com/WW/llisapi.dll/35102867?nodeid4=20229806&func=ll&objId=35102867&objAction=csView&cspltfrm=0&cssw=18&csbinh=0&lang=en&siteid=cseus&aktprim=4&extranet=standard&viewreg=WW&load=content&start=11&csSort=-DOCDATUMBEITRAG&subtype=136000 Regarding you question of layers. Layers are usefull when you draw you screens to group similar object. For example: base, slabs - layer 0 & 1 pipes - layer 2, 3, 4, 5 vessels - layer 6 pumps - layer 9 analog readings - layer 10 etc. In addition in runtime you are able to turn on and off layer and to do some animations if you want. this is only possible by using VBS! In addition layers are used when you make decluttering. Here is the link for some demo (WinCC Multitouch Gestures: Configuring and Engineering): https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid4=20229806&lang=en&siteid=cseus&aktprim=4&extranet=standard&viewreg=WW&objid=20229806&treeLang=en Best regards, yolov AttachmentGraCS.zip (734 Downloads) |
Last edited by: Yolov at: 9/24/2013 5:00 PM |
|
7/10/2014 3:36 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intocreated face plate instance, wanted to connect it with my equipments. With best regards, Narrator1
|
10/10/2017 8:55 AM | |
Joined: 6/19/2017 Last visit: 4/17/2024 Posts: 7945 Rating: (162) |
New question published by SIMANTC WINCC is split to a separate thread with the subject Need help to access structure tag in VB script. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on