11/8/2017 2:29 PM | |
Joined: 1/2/2017 Last visit: 7/11/2023 Posts: 284 Rating: (23) |
Hello all, I want to configure FM350-1 to read ifm counter with the help of the function FC CNT_CTL1 (FC 2). In the manual (S7-300 FM 350-1 Counter module Manua) page 41 it says "creadte a DB and select UDT 2 as the source file. UDT 2 was copied to the function block library called FMx50LIB when the FCs were installed". I couldnt find this UDT 2, I installed the configuration package that can be found here. but still I cant find it. any help appricated! Also anyone have a configured example to upload here. I use Step 7 v5.5 Thank you |
Disclaimer: While I strive to ensure that the content of posts and answers is accurate and complete, my posts and answers are provided “as is” and “as available.” Your use of my posts and answers content is entirely at your own risk. |
|
Follow us on