11/8/2017 8:55 AM | |
Joined: 8/25/2006 Last visit: 4/19/2024 Posts: 2203 Rating: (277)
|
Hello. Look here: Compatibility Restriction of CP50M1 & CP51M1 with D7-Sys V7.0. This restrictions are also valid for any D7-SYS version V7.0 and higher. Connect to the CPU in slot 2 and 4 via serial interface (DUST1), in CFC goto the menu 'CPU-Module Information' and read the diagnostics from both tabs (Error panels and Exception buffer) from both CPU's.
|
11/9/2017 3:48 AM | |
Joined: 12/2/2016 Last visit: 9/30/2023 Posts: 81 Rating: (1) |
Thank you at first, I have read this doc. but i do not know the really meaning of it . It tell that " The required min. hardware release for the CP50M1 module (order no. 6DD1661-0AD1) is 2. " the release is 4 for which "4" is. does mean in the version V1.1.4 , the "4" is the release number 4. |
Follow us on