6/12/2017 11:39 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
how to read digital input/output of the SIMATIC IOT2000 I/O module via node-red. |
6/12/2017 1:06 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, you can use the "intel_gpio" nodes preinstalled in the Exmaple Image. Scroll all the way down on the left hand side of your node-red. Unfortunately not all Pins are working with this nodes. To solve this problem there is a Siemens node for this. Have a look at this post: https://support.industry.siemens.com/tf/ww/en/posts/access-input-pins-user-button-and-multi-colour-user-led-from-node-red/161073?page=0&pageSize=300 Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/13/2017 11:13 AM | |
Joined: 1/25/2012 Last visit: 9/15/2023 Posts: 8 Rating: (0) |
Hi, I would like to access the I/Os via node.js. Could you provide a module for this? Best regards |
11/16/2017 12:45 PM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7954 Rating: (162) |
New question published by eric00058 is split to a separate thread with the subject What should do to make the communication protocol through IOT I/O moduel to be Modbus RTU?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on