9/19/2017 10:30 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Yes, You must configure the plant bus as an IE General card instead a CP16xx. Be aware that there are some restrictions like no more than 8 connections, no ISO only TCP/IP protocol etc. |
If I could help you, you can use the RATE button. Thank you. |
|
11/23/2017 2:56 PM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 8006 Rating: (163) |
New question published by Amen Allah is split to a separate thread with the subject The limit of 8 connections is related to TCP/IP communication or to the use of IE-General?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on