5/1/2016 11:19 AM | |
Joined: 3/28/2015 Last visit: 5/10/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: |
Eng.Mohamed Ibrahim |
|
5/1/2016 11:49 AM | |
Joined: 3/28/2015 Last visit: 5/10/2024 Posts: 721 Rating: (213) |
Hello, DP/DP Coupler and Repeater: DP/DP coupler: has two DP slave ports which can be configured with different address. The application for this is to make the data exchange with two masters. It is not a DP slave and don't need the address. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
11/24/2017 1:15 PM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
New question published by AutoGen_148962 is split to a separate thread with the subject After recycling the power of DP/DP coupler BF is not getting OK. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on