11/14/2017 8:43 AM | |
Joined: 11/24/2016 Last visit: 8/26/2024 Posts: 1 Rating: (0) |
Hi, I have an project with many connections on between my CPU and WinCC. (~4000 tags). When system is running, Plc Attributes are 0/2000 in the Channel Diagnostic. The HMI seems to work but i'm not sure if it's ok or if it could be an problem with time. I found this value in this file but i don't know the implications when all attributes are used. Does-it work or i need to reduce connections between WinCC and CPU? Any ideas? thank in advance ! (* --------------------------------------------------------------------------------------------------------------------------- *) Servers
Configuration of systems (Master/Slave) :
CPU :
|
Last edited by: Jen_Moderator at: 11/15/2017 7:23:06 AMInserted right link. |
|
Follow us on