11/12/2015 10:22 AM | |
Posts: 2930 Rating: (432)
|
Hi, to use the WEB-Server in LOGO! 8 doesn't require to have a display at LOGO! or a TDE connected. A text message is used to show information in the Web-server. What I believe is: 1. you have enabled the Web-server. In case 3: Goto the message text in LSC V8, open the properties and check if the message text is enabled for LOGO! Display. If not, then you can't see it in the Web-server if you change to LOGO! Display because it is not enabled for the LGO! display. Attached is an example you can use to understand. Ckeck the properties of the message texts for details. Once more: This example works and show messages in the Web-Server with a LOGO! 8 pure without an additional TDE connected. Hope this helps AttachmentWeb_s screens.zip (290 Downloads) |
Follow us on