11/15/2017 8:09 AM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Hi SuHu, I read though the whole thread, i do have same situation in my project, with 2 sets ( total 4 servers) of redundant server's and 11 numbers of WinCC client PC's without a dedicated domain controller. Right now Simatic Logon is not implemented in the plant. But now end client want to have Simatic logon and want to have password expired popup every 90 days. Here are few confusions, Do I need to installed Simatic Logon server's in all 4 WinCC Servers? (hope no need to install in client PC) if so, which server need to be configured to show the password expired after 90 days? If password changed in one of the sever, how the other servers will take the same password? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2017 3:07:08 PMNew subject after splitting _______________________________________________________________ |
|
12/20/2017 7:46 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
New question published by musris is split to a separate thread with the subject After installing SIMATIC LOGON 1.4 SP1 the STEP 7 project doesn't opens sometimes. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on