12/20/2017 4:32 PM | |
Posts: 10 Rating: (2) |
Hi Friends, I'm going to control a stepper motor using a PWM output. I'm using this example : https://support.industry.siemens.com/cs/ww/en/view/63200733 For axis position , I Know that the number of pulses sent to the drive needs to be controlled. I can solve my problem knowing the number of pulses sent to the drive. For example : When the number of pulses would be greater than 1000 I''ll stop the motor using another output. Is possible to count the number of pulses using PWM outputs? My system is open-loop. Best Regards . |
Last edited by: Jen_Moderator at: 12/21/2017 1:34:57 PMInserted right link. |
|
Follow us on