1/6/2018 9:29 AM | |
Posts: 241 Rating: (1) |
Attachmentac current transducer.pdf (147 Downloads) |
1/6/2018 9:32 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello hamed12580, Here NC means No Connection. User need to select CT with appropriate ration with secondary current 1/5/10A AC. CT secondary connection to be connected at terminal 2 & 3. Transducer seting to be selected depending upon CT current i.e. 1 or 5 or 10 A. Out put must be selected depending upon module selection, i.e. 0-20 mA/4-20mA or 0-10Volt. Output to be connected at output terminals as per module. HTH. |
This contribution was helpful to1 thankful Users |
1/6/2018 10:33 AM | |
Posts: 241 Rating: (1) |
if NC means no connection so i surprised why this terminal is created?! |
Follow us on