1/9/2018 6:27 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927)
|
Hi Mist9, This is done quitte easy. What you need is the internal tag: "@RM_MASTER". The internal tag exists on both servers. When the @RM_MASTER is "1", it means the server you are working on is master, when the value is "0", it means it is the standby server. You are going to need to use @RM_MASTER in a script and use this tag as If condition. Below is an example in C-script:
Good luck! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on