12/25/2013 4:33 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, no lot logical. The structure of the area pointer is different. In OP7 you have e.g picture no 1 and picture entry 1-10. In OP77B you get separate pictures. They all have different numbers. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
12/28/2013 5:28 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, to solve your problem you first must understand the differences between OP7 and OP77. I have 2 times written that the structure of the area pointer is different. In OP7 you have a screen (area pointer: Screen no). On this screen you have "sub screens" (area pointer: Screen Data entry No). After migration you have only screens, no more sub screens. When you have in OP7 screen no 1 with entry no 1-10 then you have in OP77 10 screens. It is not possible to move the data 1:1 from old area pointer to the new one. But if you edit your program first look how and if the area pointer is used. It is not useful when you push your threads with the same text. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
1/17/2018 11:56 AM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
New question published by tiendat210 is split to a separate thread with the subject Migration OP7 to OP77A. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on