1/23/2018 3:39 PM | |
Joined: 9/3/2012 Last visit: 5/1/2024 Posts: 5 Rating: (0) |
Thank you very much for the link !! I had a task to start a panel RT project on a computer for a client. It is a MP270 panel. All keys working fine, BUT.. the ACK button ?? Is there any combination for the ACK button? There is no original project for the panel, and I have only the ProTool RT file from the panel. Also great thanks toSSEfor the program It's very great one but only for WinCCFlexible, not for ProTool or TIA. Any idea how I can acknowledge the alarms as there is no ACK button in the alarms view..:( ? ------------------------------------------------------------------------------------------ |
Last edited by: stanimirstoykov at: 1/23/2018 3:41:13 PMLast edited by: Jen_Moderator at: 1/24/2018 11:55:04 AMNew subject after splitting |
|
Follow us on