1/24/2018 12:39 PM | |
Joined: 3/2/2007 Last visit: 9/18/2024 Posts: 935 Rating: (5) |
which memory card should be used with the 6SL3246-0BA22-1FA0 SINAMICS G120 CONTROL UNIT CU250S-2 PN ? which one of the following is necessary and enough to run the G120 drive ? SINAMICS G120 SD card 512 MB incl. licensing (Certificate of License) V4.7 SINAMICS G120 SD-Card 512 MB INCLUDING CERTIFICATE OF LICENCE V4.7 SP9 HF1 SINAMICS SD card 512 MB empty |
... thank you ... |
|
1/24/2018 3:40 PM | |
Posts: 13 Rating: (0) |
Hi, Ziemens! 6SL3054-7TE00-2BA0-ZE01+F01 |
1/24/2018 7:22 PM | |
Posts: 13 Rating: (0) |
yes. a card with the firmware allows you to update the software of your CU if it is obsolete |
Follow us on