1/26/2018 1:10 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
Hello FAKSARAY, are you still looking for assistance? If you are still looking for a reply my alternative suggestion is to create a Support Request and discus the issue with your local Siemens Technical Support. Thank's to the TechTeam and the other community members for sharing their knowledge Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
1/26/2018 2:00 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, here is a link to a project example. https://support.industry.siemens.com/cs/ww/en/view/109739053 You can compare with your project. When you have communication problems because EMV, you have to solve it. Check the cable. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
1/29/2018 8:14 AM | |
Joined: 3/31/2015 Last visit: 1/26/2024 Posts: 175 Rating: (16) |
Did you try changing Communication Load? Try setting it to 15% f.e. |
1/29/2018 2:52 PM | |
Joined: 3/13/2015 Last visit: 9/6/2024 Posts: 26 Rating: (0) |
No I didn't, I will try to next time anymore, because I changed the system. Thank you all for your helps and attention. |
Follow us on