10/31/2017 12:20 PM | |
Posts: 107 Rating: (0) |
Dear PCS7 users and Experts. Could someone explain (manuals and post didn't help sorry) the steps below: I've changed in my ES picture tree (add some new containers with pics) my @Area buttons PDL is user defined (not standard) so in ES everything is fine working no problem. Tried to download with picture tree update nothing except containers changed in a chaotic manner but there was no good result like in ES machine OS Project editor (I think this is the way for clients) but i'm not clear with it thanks for help IT_Service. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/3/2017 10:26:12 AMNew subject after splitting Last edited by: IT service at: 4/7/2018 9:06:29 AM |
|
11/8/2017 9:27 AM | |
Joined: 3/14/2008 Last visit: 9/24/2024 Posts: 2096 Rating: (938)
|
Hi, Normally the picture tree is generated automatically according to your plant hierarchy and plant hierarchy settings. You can define names for your buttons if you do not want to use the plant hierarchy folder names. But you have changed the picture tree on the OS server settings. If you compile and download the OS, the picture tree is generated according to your plant hierarchy again. You have to make sure you dont update the plant hierarchy when compiling the OS. |
If I could help you, you can use the RATE button. Thank you. |
|
11/8/2017 3:39 PM | |
Joined: 3/14/2008 Last visit: 9/24/2024 Posts: 2096 Rating: (938)
|
Hi, Yes correct, The clients do have a picture tree. The clients receive the server package data from the OS server containing the pictures (and more data). You can adjust the picture tree on the clients after the server data has been generated. On the client you can set the order of pictures you want to show or not to show. When you have a client with more than one server package (in case of several multiprojects), you will receive those pictures as well... It can get messed up though, like in case when you delete the server package data on the client from one of the projects. You have to run OS project editor to activate your changes to the picture tree. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on