Industry Online Support
Technical Forum
1/3/2013 1:32 PM | |
Posts: 25 Rating: (0) |
Hi All I'm working on a data logging HMI running on WinCC flexible. I'm testing it by logging a single varying voltage inputand and fan output. This program will eventually be scaled up to record data from around 30 different sensors and actuators. Im using WinCC Flexible Advanced 2008 sp3 on windows 7 and an S7-300 plc connected by ethernet. My program logs the data as a csv but the two variables appear in the same column. Is there a way to record the variables in separate columns? I have successfully used an excel macro to re arrange the data offline. However, since the program continually logs data, I need an 'online' solution. I have also tried to find an example of a suitable script with no luck. I have attached a screenshot of my csv data log file and the hmi. Could someone provide me with some advice please? Best regards and happy new year. Attachmentcsv_logger.zip (890 Downloads) |
This contribution was helpful to1 thankful Users |
8/19/2013 2:57 PM | |
Posts: 3037 Rating: (192)
|
Hello, How on a PC with WinCC flexible can you use a script to save and read out information in a text file? How on a Windows-based panel can you use a script to save and read out information in a text file? Tweety If you use this example (http://support.automation.siemens.com/WW/view/en/35929465), then you must use the german regional options. |
8/20/2013 3:36 PM | |
Posts: 15 Rating: (0) |
Hi Tweety. Thankyou for the information. Now it's working well Thanks again. |
This contribution was helpful to1 thankful Users |
2/7/2018 2:28 PM | |
Posts: 1 Rating: (0) |
Buenos días, tengo el mismo problema que tú, ¿has logrado arreglarlo? ¿usted me podría ayudar? |
Follow us on