1/25/2017 7:14 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Tony.Y, SIL2/3 safety in siemens is implemented in various modules available i.e. the same module can be used as SIL2 or SIL3 depending upon how connections are done and available of safety features in sensor or switch. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
2/3/2017 4:49 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Tony.Y, U will need to connect another similar sensor!!!!!!!!!!!! This is in definition of SIL3 to have pair of sensors. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on