2/8/2018 6:32 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, The @CPU_RT block is available as of PCS7 V7.0. The CPU410-5H will definitely support SFC 78 which is used to show the data like net consumption...With older CPU's like 416/417 you need a firmware update in order to use the @CPU_RT so I don't think this is the problem. You can check if you have I/O: MAX_RTRG set to value: "0" on the block @CPU_RT. If it is, the @CPU_RT will not show any data from the CPU. Does it show any other errors at the block outputs? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/9/2018 11:16 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi kopo, I thought you had problems with the 410-5H as well. Sorry for the misunderstanding. In this case, please check if you have the following firmware on the redundant 417-4H: 4.5 or higher. As of V4.5 you can get the diagnostic info from the CPU. PS: Just for information: If you have a single CPU, you will need firmware: V5.0 or higher Please check if you have the option: "Asset Management" as well, because otherwise certain functions cannot be used. Take a look at the attachment for an overview of functions with and without asset management option. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/9/2018 2:26 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Yes, You need to upgrade the CPU firmware to V4.5. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/9/2018 2:55 PM | |
Joined: 1/13/2016 Last visit: 8/29/2022 Posts: 37 Rating: (0) |
OK, but is this firmware version existing for this CPU? The latest which I found is the V4.0.12: https://support.industry.siemens.com/cs/ww/en/view/109474747 Thank you |
Last edited by: Jen_Moderator at: 2/12/2018 9:08:20 AMOptimized link. |
|
2/9/2018 3:12 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, you should check for your CPU what the latest firmware is. If it is 4.0, which is possible, then you cannot use the cpu_rt data. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on