2/15/2018 2:45 PM | |
Joined: 7/19/2017 Last visit: 8/27/2024 Posts: 1 Rating: (1) |
Hello I have installed PCS7 V9.0 on Win7 Proffesional (64) and tested High-precision time stamping. I have noticed that Block IMDRV_TS V9.0 from Basic library V9.0 does not work properly. When I test fast changes on DI, the messages do not appear on OS. I'm using following HW Configuration ( see picture HW-Config):
SW Config CFC (see picture SW-Config):
I have compiled CFC with generate modul drive. After compile process system chart with IMDRV_TS block was created. When i tested fast changes on DI all mesagges from MSG_TS_ET200 did not appear on OS ( see picture: Alarms_IMDRV_TS_V90). Then I used IMDRV_TS (V7.7) block from Basic Library V8.1 and everything worked fine (see picture Alarms_IMDRV_TS_V77). My question would be: Do I need some updates for PCS7 or is it the case that High-precision time stamping funcionality is not working properly with this version. Thank you in advance for the answer! Best regards! AttachmentAttacments.docx (69 Downloads) |
Follow us on