2/23/2022 8:46 PM | |
Joined: 9/17/2012 Last visit: 4/17/2024 Posts: 3 Rating: (0) |
Can anybody help? I have the same need - download to WinCC v16 RT remotely, via an ewon located on customer's site. |
2/24/2022 3:57 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1643)
|
Hello yes its possible but not that easy, you have to consider a lot of things. The most important are the settings in the SIMATIC Shell (Multicast proxy, TTL encrypted communication -> you have to see each other in the SIMATIC Shell). The Basic FAQ to loading: https://support.industry.siemens.com/cs/ww/en/view/88780011 And if it doesn´t work you can do an offline Transfer: https://support.industry.siemens.com/cs/ww/en/view/103198851 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on