3/4/2010 8:05 PM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
hmm very strange... Maybe you could check your toolbox cd... Maybe the example is on it.. and you can copy it directly to your computer. Otherwise, I don't know |
If I could help you, you can use the RATE button. Thank you. |
|
3/5/2010 8:10 AM | |
Posts: 10 Rating: (0) |
In Cd also hasn't... |
3/6/2010 8:03 AM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
topic starter has got the example project. problem solved.... |
If I could help you, you can use the RATE button. Thank you. |
|
3/9/2010 6:09 PM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
I didn't check if you had the same version as me.... sorry about that. Im not able to help you..... |
If I could help you, you can use the RATE button. Thank you. |
|
3/9/2010 7:21 PM | |
Posts: 10 Rating: (0) |
Oreca, don't worry, you have tried help me, thank you. :) |
2/19/2018 9:02 AM | |
Joined: 6/19/2017 Last visit: 4/17/2024 Posts: 7945 Rating: (162) |
New question published by Sipho is split to a separate thread with the subject need to add CU 320-2 DP on add hardware as attach. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on