2/23/2018 7:07 AM | |
Joined: 3/9/2017 Last visit: 4/27/2023 Posts: 7 Rating: (0) |
Hi, Link of pictures, --deleted Link-- Link of software, --deleted Link-- Can you please check these ? Thank you Attachmentfiles.zip (49 Downloads) |
Last edited by: Jen_Moderator at: 2/23/2018 10:33:23 AMDeleted link and added files as an attachment |
|
2/23/2018 7:09 AM | |
Joined: 3/9/2017 Last visit: 4/27/2023 Posts: 7 Rating: (0) |
Sorry not software my program that I struggle with. |
2/24/2018 5:11 AM | |
Joined: 10/28/2014 Last visit: 4/17/2024 Posts: 63 Rating: (2) |
Hi electronics26, I did observe one thing, in the modbus parameters DB you have mentioned the start address as 1. (Refer attachment). So in Modscan you should enter the start address as 2. Refer the chapter on "Address Mapping" in the manual. Also the length should be as per your program in Modscan and not the default 100. Also just to make sure it is not missed out, recheck if the connection was downloaded from Netpro! Hope this helps! |
Follow us on