8/6/2007 7:04 AM | |
Posts: 90 Rating: (1) |
SW5.0 Profile 3.1 & the existing in the plant are SW4.0 profile 3.0 Thanks for your fast reply |
8/6/2007 11:26 AM | |
Posts: 90 Rating: (1) |
Can you give me the email of Mr. Wolfgang Durr. Thanks, alibaba |
8/7/2007 1:52 AM | |
Joined: 6/13/2006 Last visit: 9/21/2023 Posts: 201 Rating: (8)
|
His email : wolfgang.duerr@siemens.com His phone number andmore information please seethe link : http://pi.khe.siemens.de/files/feldg/files/news/vi_AuD-info_SIPART_PS_en.pdf B.R chook |
[IMG]http://i17.tinypic.com/66b7jas.jpg[/IMG] |
|
7/2/2008 9:14 AM | |
Posts: 37 Rating: (2) |
dear experts, I have the same problemandI could not find the soultion for that. I require the up to date GSD file. Cheers, Mans |
7/3/2008 7:14 PM | |
Posts: 151 Rating: (8) |
Hi Mans207, already downloaded and installed the relevant files on this page? http://support.automation.siemens.com/WW/view/en/14450580/133100 http://support.automation.siemens.com/WW/view/en/10806943/133100 Good luck, SonicRanger. |
This contribution was helpful to1 thankful Users |
8/4/2008 3:04 PM | |
Posts: 767 Rating: (69) |
Hi, I ahve solved my issue with wrong version. Actually what the problem was that the transmitter is with option of profisafe (C21 for my this transmiter). The profisafe option does not change the order number but it comes as 'Z' option. you can check it on the data sheet of device. Why I wnet for it coz when I was trying to detect the deviceusing simple sitrans P DSIII GSD it was comming up with the message attached and it canbe seen clearly from the message that it is from profisafe family and when I tried profisafe GSD it detected the device and everything works ok. AttachmentError.pdf (493 Downloads) |
Follow us on