3/7/2018 8:31 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello youssef; PED, in a S7-300 or a S7-400 CPU, would designate a peripheral input double-word address. Peripheral addresses refer to any address which is outside the Input/Output image tables, which are generally used for digital addressing. So analog and communication (Profibus, Profinet) addresses use peripheral addressing. See the following FAQ for more details: https://support.industry.siemens.com/cs/ww/en/view/18325417 The "E" means input in German ("Eingang").. If your program uses English mnemonics, you would write PID (I as in Input). For Outputs , you would write PAD (in German mnemonincs, "A" as in "Ausgang") or in Eglish mnemonics PQW (Q for Ouptput). Some examples in English mnemonics: PIW256, PIB258, PID260 PQW 262, PQB 264, PQD272 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/7/2018 8:32:16 PMLast edited by: dchartier at: 3/7/2018 9:36:33 PM |
|
3/7/2018 9:19 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, |
Last edited by: Jen_Moderator at: 3/23/2018 8:19:23 AMOptimized link. |
|
3/7/2018 9:22 PM | |
Posts: 22 Rating: (2) |
thank you for your help i really appreciate it |
Follow us on