3/6/2018 11:33 AM | |
Joined: 6/5/2009 Last visit: 3/1/2024 Posts: 149 Rating: (0) |
Dear All, Attached are 2 pictures depicting the system architecture on the PROFIBUS level of communication with the ET200M I/O's and the other consists of MODBUS TCP system. Is it feasible to have multiple MODBUS TCP servers on redundant basis with a redundant S7-400 H station? If so is there any example to describe the connection and the program. Regards, Grim Reaper AttachmentSystem Architecture.zip (250 Downloads) |
Follow us on