3/8/2018 10:16 AM | |
Joined: 9/9/2009 Last visit: 11/2/2018 Posts: 2 Rating: (0) |
Hi, is it possible to use the two voltage inputs at the same time like the two current inputs ? At http://w3.siemens.com/mcms/pc-based-automation/en/industrial-iot/Pages/Default.aspx?tabcardname=simatic%20iot2000%20io-shield there are mentioned only two analogue inputs- selectable as voltage or current inputs, but the handbook https://support.industry.siemens.com/cs/ww/en/view/109745681 shows a schematic with connected all four analogue inputs. By the way - schematic is wrong at least for the current inputs because both are connected. Can I use all for inputs in parallel ? BR Falo |
Last edited by: Jen_Moderator at: 3/12/2018 12:51:24 PMOptimized link. |
|
Follow us on