1/14/2014 11:08 PM | |
Joined: 7/7/2010 Last visit: 5/10/2024 Posts: 14709 Rating: (2357)
|
I had a similar problem recently and submitted to Siemens via Support Request The answer I received was something like this, "Yeah, that happens sometimes. Changing it to Absolute is the know work-around". I urged them to forward the complaint to Siemens HQ to either note it in the documentation, or fix the problem. |
science guy |
|
This contribution was helpful to2 thankful Users |
5/23/2014 10:46 AM | |
Joined: 6/26/2009 Last visit: 4/25/2024 Posts: 122 Rating: (23) |
Hi Huggy , No useable answer from support so far. regards Koenb |
5/23/2014 10:58 AM | |
Joined: 1/5/2011 Last visit: 4/22/2024 Posts: 815 Rating: (121) |
Hi, I can confirm this problem also exsists in TiA V11 SP2 update5. It is very annoying and sometimes I can fix it by deleting the hmi tags where the bug occurs, then compile > rebuild all, then recreate them and compile > rebuild all again. It is a pain in the ass I know. |
Keep it simple and on-topic. |
|
5/14/2015 5:45 AM | |
Posts: 2 Rating: (0) |
This problem also appears with TIA v13 SP1 when i simulate PLC 1200 v4.1 with HMI 600 mono... :( |
3/20/2018 12:17 PM | |
Posts: 1 Rating: (0) |
In TIA Portal V14 is the same problem. If I change access for absolute I have connection- I mean I can for example change tag in PLC from HMI's button. But problem is if someone using optimized blocks then you can't use absolute access: Siemens Support |
Last edited by: Jen_Moderator at: 3/21/2018 10:11:27 AMOptimized link. |
|
Follow us on