3/21/2018 10:27 PM | |
Joined: 11/11/2011 Last visit: 8/11/2023 Posts: 63 Rating: (1) |
Hi I am working on an application, ET200SP 1510 CPU FW 2.1 to Sirus soft start via profinet. TIA V14 SP1, Soft Starter ES software V14 SP1 installed. I have assigned a PN name to the soft start and can go online to the device but I am unable to complete a hardware download to the PLC while I have configured a network connection between the PLC and the soft start. I can carry out the download in simulation with no issues. What I am trying to do seems so simple but I cant get past this stage. I get a message at download to check the diagnostics buffer of the target device. I have attached the diagnostics file for reference. Has anyone any experience with this? I don't see any examples on line. Thanks JT AttachmentDiagnostics.txt (64 Downloads) |
Follow us on